AXIS#.IL.VCMD
Description
Reads the output of the current loop that controls the q-component of the current.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Vrms rms stands for root mean square (also known as the quadratic mean) L-N |
Range |
0 Vrms to bus voltage |
Default Value |
N/A |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics